Figure 4-57: The Device Toolbar
| Icon | Description |
|---|---|
|
Show the controller communication properties dialog (PLC"Programmable Logic Controller"
A Programmable Logic Controller, PLC, or Programmable Controller is a digital computer used for automation of industrial processes, such as control of machinery on factory assembly lines.
Used to synchronize the flow of inputs from (physical) sensors and events with the flow of outputs to actuators and events options) |
|
Change the controller IP address to connect with KAS Simulator. In this simulated mode, the controller properties change as shown below and the Controller Type includes the IP address 127.0.0.1. |
|
|
Compile project |
|
|
Compile and download the project. This downloads the application and Project Source files. |
|
Establish connection with the target controller |
|
Close connection with the target controller |
|
Download the application to the targeted controller (note that the application must not be running). |
|
Start the application. It can be either: Warm Start (default mode): Retain Variables are loaded at the application startup. They are Not re-initialized; whereas other variables are started with their initial values. Cold Start: use retain variables with their default values. Such starts occurs from time to time but are few. To choose a Cold Start, you have to drop-down the Start button as follows: ![]() |
|
Stop the application |
If the previous download failed (due to events such as the EthernetEthernet is a large, diverse family of frame-based computer networking technologies that operate at many speeds for local area networks (LANs) being disconnected or the controller being turned off), you will not be able start your application. Additionally:
Review the Controller logs for more information.
Ensure the Simulated device mode is active (the icon
must be selected)
To establish the connection with the target controller, click the Connect Device icon
.
You need to configure the device before connecting (see Configure the Controller)
The software versions of the KAS IDE"Integrated development environment" An integrated development environment is a type of computer software that assists computer programmers in developing software. IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger and the KAS RuntimeIn computer science, runtime (or run-time) describes the operation of a computer program, the duration of its execution, from beginning to termination (compare compile time). Within KAS, runtime also refers to the virtual machine that manage the program written in a computer language while it is running have to match to avoid compatibility problems.
See KAS IDE to Runtime Compatibility for more information.
The software versions of the KAS IDE and the KAS Runtime are also available in the local log messages (the level for this message is INFO).
When another KAS IDE is already connected to the controller, a warning is displayed and the connection is discarded to prevent any conflict.
The status bar provides global information about the target and the name of the running application currently stored in the device.
Text displayed with orange background means that the version of the application is different between the KAS IDE and the target.
For more details, The following table summarizes all cases for the labels of the status bar.
Every log message has the following information:
Once connected to the device, it is no longer possible to edit the PLC programs, unless Online Change is active (see Compile the Application)
Depending on the number of AKD drives physically present in the EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs network, the KAS IDE might slow down when getting data.
The KAS Runtime is not concerned with this limitation.
|
Copyright © 2015 Kollmorgen™ |
|